Part Number: SIMPLELINK-CC13X2-26X2-SDK
Tool/software: Code Composer Studio
HI,
I'm somewhat new with Code Composer Studio. For me it seems to be a good approach of working with "working sets". I can include several projects into my workspace and select just with a working set, which project should be build.
But it seems that there is no way to put the command "Build working set" on a key of an icon in some toolbar. I always have to select the Project menu, there Build working set and then the selected working set. This is some clicking. Preferably I can put this command on a function key or/and an icon item I can put into a toolbar.
Or is there another possibility to identify a project somehow as "active project" so that this would be build doesn't matter which item is currently selected in the Project Explorer?
Thanks in advance
Erwin