The Ducati team asked me to post this here to get an answer on why we are seeing difference between Linux and Windows builds in the code section.
See email excerpt below and attached files...
I am attaching
the section wise breakup of three images buillt on different machines (by
different members of our team) which have the same versions of the tools and
also the same version of the Ducati Syslink code (built only once).
There is a
difference in the code section of the Ducati image that is built on Windows and
Linux. The size is very small (12 bytes) - Will need the compiler team to
investigate this discrepancy.
Regards,
Amith Dsouza