Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi,
I'm programing my cc3220SF custom board with a CC3220SF-LaunchPad
I program my custom board with uniflash using the Out of the box zip. The service pack is simplelink_cc32xx_sdk_4_10_00_07. I'm erasing the mcuflashimg.bin file from the user files to be able to debug my program.
I have my custom board with 010 SOP configuration.
The divice is in development mode.
With CCS, I try to debug the out of the box code or an empty proyect (Freertos version), I'm getting the following error on CCS:
Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
I followed this article but I use the latest sdk and have de SOP on the 010 position and the device is in development mode.:
software-dl.ti.com/.../ccsv7_debugging_jtag_connectivity_issues.html