Part Number: TMS570LS3134
Tool/software: Code Composer Studio
Hello,
I have a project that can be compiled to two different TMS570LS31 (34 and 37, but it is not important). I have done that succesfully, compiled and ran the code etc.
I am now doing a few steps to make the code easily available to others in the company. Anyway, I am doing checkout, configuration and compilation steps from scratch.
I thus have two Debug Configuration, one oriented towards 3137 and the other to 3134. The 3137 builds without any problem, but the 3134 produces a compilation error (unresolved symbol, linking error #10234-D) for three function symbols. These functions are inlined. I noticed that if I remove the inline symbol, the compilation completes without any problem.
Problem is: I do not want to modify the code to be able to build (besides the fact that I successfully built it in another project before).
I do not see an obvious difference between both my build configurations (other than some defines and specific file linking for 3137/3134 HAL code that do not come in play in that error).
Do you known what I can do about that ?
Regards
Christophe