This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C123AE6PM: While building using Command line giving some error

Part Number: TM4C123AE6PM
Other Parts Discussed in Thread: CCSTUDIO

Tool/software: Code Composer Studio

HI,

As am working on some personal projects.

am trying to compiling and building using some Perl script added below commands to generate binaries. when I run into local it was working fine ( binaries creating ). the same script using it into the server ( bamboo ). when I triggered the server not able to generate binaries. same time if I open ccs and observe there is some error it is throwing in the related to work space.

Error:

An internal error occurred during: "Periodic workspace save.".

Cannot set lower sequence number for root ( previous: 103, new: 102). Location> c:\projetos\projetosCCSV6\TM4C123AE6PM\.metadata\.plugins\org.exlipse.core.resources\.safetable\org.eclipse.core.resources

Commands:

'eclipsec -noSplash -data '.$CODE_DIR.' -application com.ti.ccstudio.apps.projectImport -ccs.location '.$PRJ_LOC.' -ccs.autoImportReferencedProjects >> '.$PROJECTS[0].'_Import_log.txt';

'eclipsec -noSplash -data '.$CODE_DIR.' -application com.ti.ccstudio.apps.projectBuild -ccs.projects '.$_[0].' -ccs.buildType full -ccs.configuration '.$_[1].' >> '.$_[0].'_Build_log_'.$type_of_config.'.txt';

can anyone help on this?

Details:-

Mictorcontroller :- TM4C123AE6PM

IDE:- CCS 6.0

Best,

Ugra