Part Number: CC2642R
Tool/software: Code Composer Studio
Hi,
CC2642R Launchpad is flashed with cc26x2r1lp_bim_onchip first and then flashed "simple_peripheral_oad_onchip_app_CC26X2R1_LAUNCHXL_tirtos_ccs" to verify the secure boot
After flashing device went to unknown state , now we are not able to flash any application as device is not detecting
Getting below error for reflashing any application
Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 8.4.0.00006)
Please help me recovering the device
Regards,
shilpa