Part Number: TMS320C5504
Other Parts Discussed in Thread: OMAP5912
Tool/software: TI C/C++ Compiler
We are trying to migrate a project, which was previously built on Code Composer v3.3, over to being built on Code Composer v10.0. The project generates an a00 ASCII hex file that is placed into the TMS320C55x DSP located on an OMAP5912. The project does successfully compile using Code Composer v10.0, using C5500 Code Generation Tools 3.3.2 provided from TI, but the project generates a binary that differs from the one generated on Code Composer v3.3. In addition, and most importantly, this newly generated binary fails to run on the DSP.
We copied the C5500 compiler tools from the Code Composer v3.3 install, and produced the same results, on Code Composer v10.0, when using the C5500 Code Generation Tools 3.3.2. Thus, we feel this rules out the compiler tools as the source of the issue.
Currently, the Code Composer v.10.0 project uses XDAIS v6.24.1.6, and the Code Composer v3.3 project uses XDAIS v2.24.x (I don't recall minor version, though I can get it if useful). Could the XDAIS version disparity be the source of the binary generation issues we are having? What other tools, if any, play a part in generating the a00 binary file in Code Composer v10.0?