Part Number: CC1312R
Other Parts Discussed in Thread: UNIFLASH,
Tool/software: Code Composer Studio
We are using Uniflash v6.0.0.2710 and IAR Embedded Workbench v8.3 with XDS110 to develop on CC1312R. We are trying to synchronize the EMU pack between UniFlash and IAR so that we don't have to update the XDS110 firmware every time we switch between the tools.
The Uniflash v6.0.0.2710 comes with EMU Pack v8.4.0.00006, and IAR Embedded Workbench uses EMU Pack v8.1.0.00005.
Questions:
- Is it possible to downgrade UniFlash v6 to use EMU Pack v8.1?
- If 1) is not possible, is there an earlier version of UniFlash that uses EMU Pack v8.1 and is compatible with CC1312R?
- This one is less critical and may not be better asked on IAR forum... is there a way to upgrade the EMU Pack associated with IAR Embedded Workbench or is this fixed per installation of that IDE?
Thanks,
Ruben