Other Parts Discussed in Thread: CODECOMPOSER, SW-TM4C-IQMATH
Tool/software: Code Composer Studio
I'm resurecting an old project that used TivaWare_C_Series-2.1.0.12573, I downloaded TivaWare™ for C Series IQ Math Standalone Package which is v2.2.0.295. How is this installed and built? I unzipped it to the TivaWare root and that seems correct because after running gen_source.pl CodeComposer can find IQmathLib.h but now I get this:
gmake: *** No rule to make target 'E:/Programs/ti/TivaWare_C_Series-2.2.0.295/IQmath/ccs/IQmathLib/Debug/IQmathLib.lib', needed by 'XXXXXXXXX.out'.
gmake: Target 'all' not remade because of errors.
How do I build IQmathlib.lib? The makefile in the IQMath folder is looking to build Makefile.IQmathLib but that file doesn't exist. CodeComposer can't find a project in the subdirectory and the readme.txt simple has "This project will build the Tiva IQmath Library." but nothing about how that is actually done. All documentation I could find is written for different versions and the section on installation just gives the directory structure of the unzipped files but not actual information.
Can anyone help?