I am currently evaluating CCS V4.2.1.
For this I imported an existing project which was made some time ago with CCS V3.1. I rebuild all, however the linker outputs that the section .econst does not fit into the flash memory of the used F2812. However that is possible with CCS V3.1. The code generation tools are 4.14 (V3.1) and 5.29 (V4.2.1).
The project settings seems the same, I have not changed them after the project import. I do not assume that the new code generation tools are less efficient, maybe the project settings need some change. The optimisation level is set to 3 in both cases.
Any ideas are welcome ;-)