This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: CC2640R2

Part Number: CC2640R2F

Tool/software: Code Composer Studio

Hi 

I am trying to find older version of SDK on Resources explorer but it is not updating even after installation.

screenshot is attached

I want SDK 3.40.10 version

thanks

  • Muhammad,

    I can show the procedure for displaying older versions of SDK in Resource Explorer.  However there is a bug that is preventing this from working.  This issue will be resolved with the release of CCSv10.1.  That said the release is online and will fix CCSv10.0 as well.

    To install an older package you can select the SDK, click on the 3 virtical dots to bring up the context menu.  Select Manage Versions.

    You can then see older versions of the SDK.  On the right you can click on the arrow and choose to install them.  The check box on the left controls which versions are displayed in Resource Explorer.  The check box on the left is not currently working.

    To import an example from the SDK today you would need to go to the Project menu and select Import CCS Projects.  Then browse to where the SDK is installed.  

    Regards,

    John

  • Hi John 

    Thanks

    I tried to import CCS project. I Got this error

    ¨¨Import failed for project 'tirtos' because its meta-data cannot be interpreted. Please contact support.¨¨

    how can I fix this 

  • Muhammad,

    Can you let me know which example project you are importing so that I can try to reproduce?  It sounds like the SDK installation may be corrupted.

    I am going to loop in our project expert as well.

    Regards,

    John