Hi,
I am using a TMP570LS with XDS100v2 JTAG; however, in CCS4.2, I do not have the option for the "clock" (under target). Any suggestion/comments on why this is happening?
Thanks,
Ariton
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using a TMP570LS with XDS100v2 JTAG; however, in CCS4.2, I do not have the option for the "clock" (under target). Any suggestion/comments on why this is happening?
Thanks,
Ariton
Ariton,
The clock options only show up if the emulation driver is exposing events that can be counted (typically only cycles). If nothing is being exposed then the clock feature will not be available. If you use another emulator is clock available?
I can try to find a TMS570LS on monday to test.
Regards,
John
Many thanks John,
if there is a fix, it would be great, as I won't have to look at the register for the free counter and covert the values.
Regards,
Ariton