Part Number: TDA2HV
Tool/software: Code Composer Studio
Hello!
My question is as follows:
When programm crashed, like this:
[CortexA15_0] MAC Port 0 Address: 00-35-ff-ad-15-f8 Phy Status: Phy 1 found on MAC port 0 Network Added: If-1:192.168.1.4 Link Status: 1000Mb/s Full Duplex on PHY 1 Create CLIENT After TaskCreate() RUN!!! ----- SendClientTCP start work Exception occurred in ThreadType_Task. Task handle: 0x89925bc4. Task stack base: 0x89926628. Task stack size: 0x2000. R0 = 0x89928515 R8 = 0x8992bc30 R1 = 0x8992bf42 R9 = 0x89928fa0 R2 = 0x8992bf42 R10 = 0x00000000 R3 = 0x00000070 R11 = 0x89925ef8 R4 = 0x84000016 R12 = 0x8992bf40 R5 = 0x84240000 SP(R13) = 0x89839af8 R6 = 0x8992bf0c LR(R14) = 0x8992bb6c R7 = 0x89929e28 PC(R15) = 0x89839af8 PSR = 0x89928fa0 DFSR = 0x00000221 IFSR = 0x00000000 DFAR = 0x8400002e IFAR = 0x00000000 ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x89839af8, lr = 0x8992bb6c. xdc.runtime.Error.raise: terminating execution
How to interpret the displayed information? What does it mean?