Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138: HPI Boot Start Address with GNU Compiler

Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138

Hi there,

I am using gcc v7.1 as my compiling toolchain. I am running into trouble with HPI Boot: If booted via HPI, the TI Bootloader expects an 4-Byte address (Program Entry Point) on 0x80000000. At the end of HPI Transfer, TI Bootloader reads the program entry point address from 0x80000000 and branches to it.

In our old Keil ARM Toolchain, it was a simple Task to write this Address to 0x80000000 in Assembler Startup File:

                AREA    Start, READONLY
                DCD     Start_Prog

Start_Prog is the Program Entry Point, DCD reads the address, Section Start is loaded to 0x80000000.

Is there an equivalent to DCD in GNU assembly syntax? In ARM Docs it says one can use .word Start_Prog, but this configuration does not work for me

Best Regards,

Chris

  • Christian,

    We are only supporting TI ARM toolchain for development on ARM9 in OMAPL138 so I am not able to provide any guidance here. I am moving this to the compiler forum if the toolchain champs there can provide any guidance on this topic.

    Regards,

    Rahul