Part Number: TMS320F28054F
Tool/software: Code Composer Studio
I'm having issues running a program using a dashboard project in GUI Composer. I am using the XDS100v3 JTAG debugger, and all settings appear to be configured correctly. The board connects successfully and says the program has downloaded, but it does not run. Sometimes (but rarely) it will work after I press the reset button on the board and restart the program. The program runs fine from Code Composer Studio.
My GUI only contains a simple dial with its value binded to a variable in the program. When the program is working, I can change that variable with the dial.
Not sure what the problem could be, TI Cloud Agent seems to connect fully. Do I need CCS Cloud or something else that I'm missing?
Thanks