This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 v6 Beta code gen tools fail to install in CCS V5 on linux

Hello,

I am trying to set up ccs5 to work with the new f2806x picolo control stick. However, I get the following error message:

 

Cannot complete the install because some dependencies are not satisfiable
  com.ti.cgt.c2000.6.0.feature.group [6.0.0.BETA1] cannot be installed in this environment because its filter is not applicable.

Any hints on how to fix this?

  • Henry,

    When does this message come up?  Is this when you are installing the compiler or when trying to configure CCS to use the compiler.  I believe CCSv5.0.1 has the 5.2.9 compiler in it.

    Where did you get the linux version of the 6.0 compiler?  Was it via the update manager in CCS?  I am wondering if this is actually pulling down the Windows package and not the Linux one as I don't think we have started posting an Linux compiler packages via update manager yet.

    Regards,

    John

     

  • JohnS said:

    Henry,

    When does this message come up?  Is this when you are installing the compiler or when trying to configure CCS to use the compiler.  I believe CCSv5.0.1 has the 5.2.9 compiler in it.

    Where did you get the linux version of the 6.0 compiler?  Was it via the update manager in CCS?  I am wondering if this is actually pulling down the Windows package and not the Linux one as I don't think we have started posting an Linux compiler packages via update manager yet.

    Regards,

    John

     

    This happens when I try to install the compiler via the update manager. Is there an error log I can look at to see if it is trying to pull down the windows version?

  • When it is downloading the update it will show the name of the file being downloaded. Below I can see that my windows install is downloading an exe.

    I took a look at the update site backend and I only see the exe on it.  I don't see a package for Linux.  We may not be ready to send out updates for Linux with these early releases yet.  I will try to track down a Linux package for the C2000 6.0 compiler and I will send you a private message with the link.

    Regards,

    John

     

  • Yes it looks like we are not ready for doing updates for Linux yet.  I will file a defect to track this.  In the mean time I send you a private message with a link to the Linux installer for the compiler.  The message will come in the form of a friend request.

    Regards,

    John