This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR4133: Power (ULP) Advice does not recognize an unsigned char

Part Number: MSP430FR4133

Tool/software: Code Composer Studio

I have the following code:

void D5TE_getData(uint8_t *data)
{
	uint8_t i;

	for(i = 13 ; i > 0 ; i--)
	{
		data[13 - i] = rxBuffer[13 - i];
	}
}

and the next advice:

#2553-D (ULP 14.1) Array index (involving "i") of type "int". Recommend using "unsigned int" 

can you tell me why it doesn't recognize the unsigned char since for me it doesn't make sense to put an unsigned int for the

amount of values that are here, I should delete this tip or there is something that I could do