Part Number: INA3221
Tool/software: TI C/C++ Compiler
Hi i need a coding support for INA3221 And LP875765
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA3221
Tool/software: TI C/C++ Compiler
Hi i need a coding support for INA3221 And LP875765
Hi,
INA3221 will not be able to take instructions from any C/C++ compiler directly.
A search on “LP875765” came up empty; however if this is a controller you’re using, please contact its vendor for advice on a proper compiler.
Regards, Guang
Had some doubts regarding ina3221
the default values og channel 1 alert limit register is FFFh but as the requirement i need to set alimit of 5 v how to do that?
For LP875765 i need to configure as 2 phase 2 output how can i do that?
Could you please help me out
Hi,
“LP875765” is not a valid part number; you may want to check.
To write to INA3221, you can refer to datasheet section 8.5.2. Specifically the figures (27, 28) show the implementation.
It is up to you to choose a controller if you don't have one already. INA3221 can work with any as long as the above communication protocol is used. Further the controller you choose determines the “compiler” needed.
Regards, Guang