Part Number: AWR1243
Tool/software: Code Composer Studio
Hi TI team,
Recently, we tried to calibrate the radar with the reflected corner put at 5 m as you mentioned in datasheet.
But we think the distance 5 m is still in the near field as using the 86 antenna.
Isn't there an extra phase exist between each antenna as the target at the far field ?
We find the angle of azimuth and elevation at far field will be wrong after the calibration is done.
But if we do the calibration by put the corner at far field (R~15m), the angle of azimuth and elevation at far field are correct and stable.
We want to know how you team do the calibration at near filed and the angle of azimuth and elevation are still correct at far field.
Thank you so much.