Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDX654IDKEVM: cannot load program onto A53 Core 0

Part Number: TMDX654IDKEVM

Tool/software: Code Composer Studio

Hi,

I have created a sample project with a minimal main.c that compiles and creates an .out file. However, when I try to debug and upload it via jtag onto A53 Core 0, it tells me

"Device functional clock appears to be off. Power-cycle the board..."

I have no idea what to look for. I have set the boot mode to 'sleep - no boot - debug', SW3[0..3] = 0000 and this did not help

Initial jtag configuration and connection verification works.

KR

Andreas