Tool/software: Code Composer Studio
Hi,
We were using CCS V8 so far and decided to switch to CCS V9 (9.3.0) as we intend to use the newly added processor from the C2000 delfino family.
After the install, I have created a new workspace. However, when I restart the software it crashes (see log).
It seems the software is trying to run an executable from a folder inside my user folder.
The problem is that our IT is using AppLocker and restrict execution to a set of directories (such as C:\ProgramData for example) and the user folder is obviously not an allowed one.
What is also odd is that if I uses the workspace I used to have for the V8 with the V9, it doesn't crash.
This is really problematic for us.
Thanks in advance,
Clément