Other Parts Discussed in Thread: OMAP3530, DM3730
We use XDS560. There is no OMAP3730 for selection in CCS setup. Which version of CCS starts to support this chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
DM3730 is the sister device of OMAP3630 and a very similar device to OMAP3530, therefore you can configure it for any one of them until CCS provides the complete package.
Check the page below that contains an example target configuration file and GEL files for the DM3730.
http://processors.wiki.ti.com/index.php/OMAP_and_Sitara_CCS_support
Hope this helps,
Rafael