Hello,
after updating the CCSv4 to vesion 4.2.1.00004
(Help -> Software Updates -> Find and Install... -> Search for updates of the currently installed features)
the Search Results offers me to install the following features:
- IPC 1.21.2.23
- RTSC/XDCtools 3.20.7.86
- SYS/BIOS 6.30.3.46
I downloaded then the bios_setupwin32_6_30_03_46.exe and xdctools_setupwin32_3_20_07_86.exe from TI download pages and installed them maually.
The new BIOS and xdctools were installed successful directly in the default folder:
C:\Program Files\Texas Instruments
When I now run the Software Updates again, CCS4 still offers me the above 3 features.
The folder in which the CCS4 will install (for example the new BIOS) is:
C:\Program Files\Texas Instruments\ccsv4\eclipse
What is the correct folder for installation?
As I already have installed two features, how can I bring the CCS4 not to offer me the installed features again?
As I don't need/use the IPC, is there a way to supress IPC in the Software Updates?
Thanks,
Frank