Tool/software: Code Composer Studio
Hi Team,
I have downloaded mmwave_automotive_toolbox_3_0_0__win and mmwave_sdk_03_02_00_04. I have imported Beam steering projects(2 project) to CCS from automotive toolbox.
First I did build of DSS project and it was successful.
Then I started to build MSS project.For that ,the build is not getting completed.The size of the xwr18xx_mrr_demo.bin file gets increasing while build is ongoing.
The build is at 39% in CCS.
If I force-stop the build, I am getting the error like,
Error: Program "C:/ti/ccs/utils/bin/gmake" is not found in PATH
I need to build this MSS project and I need to test mrr_beamsteering in automative toolbox.
Please help me in solving this.