Part Number: DP83848I
Tool/software: TI C/C++ Compiler
Hello,
I am using STMicroelectronics' CPU and doing Ethernet communication using DP83848IVV.
I am using MAC address in DP83848IVV through source coding.
1. Is the MAC address individually built into the DP83848IVV chip??
2.If the MAC address is individually embedded in the chip, is it okay to use it in the production line without purchasing the MAC address separately from the IEEE Registration Authority?