Part Number: C2000-CGT
Tool/software: Code Composer Studio
Hi Ki,
I have three imported CCS 3.3 projects in CCS 10.0 now. Two of them are the child projects serving to the top level application project - so I can open them inside this top level app project as "Project Dependencies" inside CCS 10. When I build each of two child project independently using the latest tool (20.x), it built successfully. But the problem is when I build the top project which relies on these two sub-projects, it failed build and points to an incorrect default location for .OBJ which, BTW, I thought to have already corrected in advanced option using directory specifier for each dependent project build earlier. I don't know where in CCS 10 do I overlook to have caused this build failure. Guess you might know.
Thanks Ki in advance! BR.