This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320DM8168: NAND FLASH : Verification failed: Values at address 0x80000000

Part Number: TMS320DM8168

Tool/software: Code Composer Studio

Hi All...

we are working on the designed a evaluation board with TMS320DM8168.

So for NAND flashing we are using the CCS7 utility. Now it can be correctly connect  board to system using XDS100v2 JTAG controller, and also can be initialized with default gel files which

in the EZSDK(/ti-ezsdk_dm816x-evm_5_05_02_00setuplinux).

I follow the all steps given by this link

So after uploading the Gel file,when we load the nand-flash-writer.out file we got the bellow error


CortexA8: File Loader: Verification failed: Values at address 0x80000000 do not match Please verify target memory and memory map.

CortexA8: GEL: File: /home/demo/Desktop/Untitled Folder/nand-flash-writer/NETRA/Debug/nand-flash-writer.out: a data verification error occurred, file load failed.

IcePick_D_0: Power Failure on Target CPU: (Error -180 @ 0xFFFFFF4C) The controller has detected a target power loss. The user must turn-on or connect the power supply for the target. (Emulation package 7.0.48.0).

CortexA8: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  

It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

 

Why occurs this ?

I need to modify the DM816x.gel ?

we are using XDS100v2 JTAG controller so is it capable for DM8168 !

Thank you, 

Best Regards,

Anilk. Dongare