Part Number: TMS320F28379D
Tool/software: TI C/C++ Compiler
Greetings,
I have a linker command file with an error in it where two areas ended up overlapped in memory. But this situation did not produce a linker error. The relevant part of the MEMORY piece of the cmd file looks like this:
MEMORY
{
PAGE 0 :
EXE_RAM : origin = 0x008800, length = 0x001000
PAGE 1 :
BUFFER : origin = 0x008800, length = 0x001800
}
As the name implies, EXE_RAM holds code which is executed from RAM. BUFFER is used for buffers, and the code which uses it overwrites the executable code which is placed in EXE_RAM when the system powers up. Obviously, this is an error which I will be fixing. But I would have expected the linker to give me an error.
What do I need to do to have the linker generates an error in this circumstance?
Thank you,
Ed