Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software: Code Composer Studio
i have two TM4C1294NCPDT launch pad i want to establish CAN communication between this boards, i have 2Nos MCP2551 Transreciver i am using example code simple_tx.c and simple_rx.c i imported hello example project and just replaced hello.c by simple_tx.c i am getting some errors which i couldn't resolve please help me to resolve the issue or if any related code or project will be helpful thank you..
gmake: *** [hello.obj] Error 1
'Building file: ../startup_ccs.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/include" --include_path="c:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl" --include_path="c:/ti/TivaWare_C_Series-2.1.4.178" --advice:power=all -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=TARGET_IS_TM4C129_RA0 --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --ual --preproc_with_compile --preproc_dependency="startup_ccs.d" "../startup_ccs.c"
"../startup_ccs.c", line 229: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../startup_ccs.c", line 247: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../startup_ccs.c", line 265: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
'Finished building: ../startup_ccs.c'
' '
'Building file: C:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl/drivers/pinout.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/include" --include_path="c:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl" --include_path="c:/ti/TivaWare_C_Series-2.1.4.178" --advice:power=all -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=TARGET_IS_TM4C129_RA0 --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --ual --preproc_with_compile --preproc_dependency="drivers/pinout.d" --obj_directory="drivers" "C:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl/drivers/pinout.c"
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13832: warning #48-D: incompatible redefinition of macro "GPIO_PA2_SSI0CLK" (declared at line 2354)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13837: warning #48-D: incompatible redefinition of macro "GPIO_PA3_SSI0FSS" (declared at line 2356)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13875: warning #48-D: incompatible redefinition of macro "GPIO_PB2_I2C0SCL" (declared at line 2372)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13879: warning #48-D: incompatible redefinition of macro "GPIO_PB3_I2C0SDA" (declared at line 2375)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13970: warning #48-D: incompatible redefinition of macro "GPIO_PF0_TRD2" (declared at line 1900)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13975: warning #48-D: incompatible redefinition of macro "GPIO_PF1_TRD1" (declared at line 2479)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13979: warning #48-D: incompatible redefinition of macro "GPIO_PF2_TRD0" (declared at line 2483)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13983: warning #48-D: incompatible redefinition of macro "GPIO_PF3_TRCLK" (declared at line 2488)
"c:/ti/TivaWare_C_Series-2.1.4.178/driverlib/pin_map.h", line 13988: warning #48-D: incompatible redefinition of macro "GPIO_PF4_TRD3" (declared at line 1922)
"C:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl/drivers/pinout.c", line 324: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
'Finished building: C:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl/drivers/pinout.c'
' '
'Building file: C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/include" --include_path="c:/ti/TivaWare_C_Series-2.1.4.178/examples/boards/ek-tm4c1294xl" --include_path="c:/ti/TivaWare_C_Series-2.1.4.178" --advice:power=all -g --gcc --define=ccs="ccs" --define=PART_TM4C1294NCPDT --define=TARGET_IS_TM4C129_RA0 --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --ual --preproc_with_compile --preproc_dependency="utils/uartstdio.d" --obj_directory="utils" "C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c"
"C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c", line 668: remark #2623-D: (ULP 5.4) Detected an assignment to a type with size less than int. To avoid unnecessary sign extension, use int-sized types for local varaibles and convert to smaller types for static storage.
"C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c", line 878: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c", line 1044: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c", line 1139: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c", line 134: remark #1534-D: (ULP 7.1) Detected use of global variable "g_pcHex" within one function "UARTvprintf". Recommend placing variable in the function locally
'Finished building: C:/ti/TivaWare_C_Series-2.1.4.178/utils/uartstdio.c'
' '
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
PROBLEMS:-
Description Resource Path Location Type
#167 too few arguments in function call hello.c /hello line 269 C/C++ Problem
#18 expected a ")" hello.c /hello line 269 C/C++ Problem
gmake: *** [hello.obj] Error 1 hello C/C++ Problem
gmake: Target 'all' not remade because of errors. hello C/C++ Problem