Part Number: TMS320C6713B
Tool/software: Code Composer Studio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6713B
Tool/software: Code Composer Studio
Hello,
It sounds like you are using a customer board. Is that correct?
In any case, there was some failure with CCS/emulator communication with the target. But I would like to check that the blackhawk emulator is correctly enumerated on your PC. You can use the Blackhawk Control Panel (see page 23 of: https://www.blackhawk-dsp.com/downloads/docs/appnotes/BH-Troubleshooting-UG-03.pdf). If that looks ok, please try running a basic scan as mentioned in page 34. If that also passes, then it seems like low level connectivity is ok.
Also, have you been able to connect to this board in the past using the same setup?
Thanks
ki
Thanks ki
It sounds like you are using a customer board. Is that correct?
answer:Yes. That's right.I have implemented TMS320C6713B on the customer board.
Also, have you been able to connect to this board in the past using the same setup?
answer:Yes.I made 10 customer boards and only one error occurred.In some cases, the board with the error can be connected.