This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Trouble connecting putty to output

Part Number: CC2640R2F

Tool/software: Code Composer Studio

I'm new to CCS and this board. I recently changed around my files on my computer which I believe is the problem here. I used to be able to load simple peripheral or project zero onto the board and turn the LEDs on and off from different apps (nRF Connect, TI sensortag, etc). I also used to be able to see connection data on putty. I rearranged my files, but recopied my workspace files where they were before. Now I can flash the board, but no data is written to putty and I can no longer change the LED values or register button pushes. When the board flashes the CCS output is:

Cortex_M3_0: GEL Output: Memory Map Initialization Complete.

Cortex_M3_0: GEL Output: Board Reset Complete

Any help would be appreciated!

  • Are you sure you are telling putty the correct serial port?

    Does the terminal work inside CCS?

  • Keith - Thanks for your reply. The terminal is not showing anything inside CCS and I also cannot discover the device via bluetooth on my phone or tablet as it was before.

  • Hi Olive,

    I'm assigning your post to an expert to assist. 

    It may be good to mass erase your device and then flash it again with the prebuilt Project 0 hex and retest though. If this isn't successful, i think you would need to load the project and use the debugger to assess if the device is in a spin lock or something. 

  • Hi Evan -

    Thanks. I did that and it seems as if Project 0 works fine and what I'm attempting to do (add a characteristic to a service for BLE applications) is causing the problem and sending this error:

    Error initializing emulator:
    (Error -260 @ 0x0)
    An attempt to connect to the XDS110 failed.
    The cause may be one or more of: no XDS110 is connected, invalid
    firmware update, invalid XDS110 serial number, or faulty USB
    cable. The firmware and serial number may be updated using the
    xdsdfu utility found in the .../ccs_base/common/uscif/xds110
    directory of your installation. View the XDS110SupportReadMe.pdf
    file there for instructions.
    (Emulation package 9.2.0.00002)

  • Hi Olive,

    You can find some information about this error on the TI Resource Explorer located at Dev.ti.com if you go to Development Tools->Debug Probes->XDS->Documents->JTAG_Debugger Connectivity Issues. If you then look for the error you have (-260) we can see that this issue is likely caused by a faulty USB connection. In order to isolate where the issue is, I've listed a few steps below that you can try. I've ordered them from least-complex to most-complex to make it easier for you. 

    1. Try a different USB port on the host computer. This is pretty unlikely to be the issue, but it's worth a try due to how simple it is.

    2. Try a different cable to connect your computer to the board.

    3. Try a different board/launchpad, if you have one. This will help determine whether the board was damaged.

    4. Open the document named "XDS110SupportReadMe.pdf" located at **Your CCS Install location**\ccs\ccs_base\common\uscif\xds110 . In this document there is a section titled "Recovering a Bricked XDS110 without JTAG". Try following these steps to try to recover the XDS110 device located on your board.

    Best Regards,
    Alec M