Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello there
I hope you all are safe and healthy. I am working on Two-Phase Interleaved LLC Resonant Converter by using TMS320F28379D. It is dual-core so it has CPU1 and CPU2 so I am planning to use both CPU for two different LLC converter for two different applications (later will use for LLC {CPU1} control and another application {CPU2}). As per its multi-day workshop in LAB11, it is mainly related to IPC but didn't mention that how to operate 2 same or 2 different projects by using dual-core. As per the pdf of TI, I'm following the example of the LLC controller (an example is given under this name 'HV2PHILLLC' Location of this folder will be ..\controlSUITE\development_kits\TIDM_1001\v1_00_00_00\f2837x\HV2PHILLLC). I have added HV2PHILLLC as a project 1 (which should run on CPU 1) and duplicate that with HV2PHILLLC2 as a project 2 (which should be run on CPU2). For that, I have set up cpu2 in debug but it won't change. Does TMS320F28379D has feature to control dual project at the same time? If yes then how can I set each project at specific CPU 1 or 2?
Please stay safe
Thank you
Avi P.