This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: Ubuntu Linux 18.04 with Linux gcc

Tool/software: TI C/C++ Compiler

ti-processor-sdk-linux-rt-am57xx-hs-evm-06.03.00.106-Linux-x86-Install.bin

After installed this SDK under Ubuntu Linux 18.04, then I created a cross compiler sw with my application code on it, can I use this image to support either am574x GP or am574x HS on the target devices?  If yes, can I just use digital sign or not on boot loader to determine the SH code in use or not?     I expect that same software could work on my devices can have either am574x or am574xhs,