This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28388D: How to edit and use Build Configuration in CCS V10

Part Number: TMS320F28388D

Tool/software: Code Composer Studio

Hi There,

I am using CCS V10. I was looking to edit the build configuration settings in CCS.

1. How to edit the Build configuration

2. How to link between the functionality and the configuration written in that.

I could not relate and change the configuration. i see only name and description. However, in the example program, it has options called RAM and FLASH, based on which it selects the RAM mode or FLASH mode.

Any guidance is appreciated.