Tool/software: Code Composer Studio
To Carry out different binaries are loaded to work my project successfully 1st Binary is loaded in SECTOR 1 , 2nd Binary in SECTOR 2 , 3rd Binary in SECTOR 3 , 4th Binary in SECTOR 4 ... etc ......
I am using CCS 5.5 and doing multiple projects in my workspace , during loading to the TMS570LS3137 .
This requires that the Flash settings are changed as required for required Project . Once I save the Flash setting for project 1 , 2, 3, 4 it is ok that the changes are saved on my PC but if someone else picks-up my Flash settings project in HIS PC the Flash Settings are not restored with what I saved it is defaulted ---- question is where and which file saves the FLASH SETTINGS FOR CCS .