Other Parts Discussed in Thread: CCSTUDIO
Clean Install of CC3.3 and the latest & proper drivers from spectrum digital for the 510PP+ jtag.
SDconfig sees the pod and I can connect properly to the target from CCstudio.
When I go to use the F28xx On Chip Flash programmer, I select the correct items in the FLASH settings, chip type, flash api, etc.
The chip is not reported as unlocked, and I can program the target via other means (see below)
When I then click program, the F28xx On Chip Flash programmer dialog greys out and then nothing happens. No progress is shown in the bottom window.
The F28xx On Chip Flash programmer dialog remains greyed out, even if I close it and re-open it and reconnect to the target. I have to restart CCS to try again.
I have confirmed the plugin is installed correctly using the component manager.
Now, I have another laptop that is configured with CC3.1 and it works fine with the same pod and target. I can also program the flash using the serial boot loader
This all started because I am upgrading my laptop at work, so I thought I would also upgrade to CCS 3.3 at the same time.
Any help much appreiciated.