This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

assertion error

i am using tda2xx & created an algorithm link (DSP1)  (non in place) 

while testing the appimage i got the below error:

ALGORITHM: Create in progress (algId = 1) !!!
[DSP1 ] 16.641981 s: Assertion @ Line: 332 in image/algPlugin.c: pSystemVideoFrameBuffer->bufAddr[0] != NULL : failed !!!
[DSP1 ] 16.642255 s: Assertion @ Line: 332 in image/algPlugin.c: pSystemVideoFrameBuffer->bufAddr[0] != NULL : failed !!!

this error is in create function of algplugin.c file

pSystemVideoFrameBuffer->bufAddr[0] = Utils_memAlloc(UTILS_HEAPID_DDR_CACHED_SR,(maxHeight*(pimageObj->pitch)*2),ALGORITHMLINK_FRAME_ALIGN);

 UTILS_assert(pSystemVideoFrameBuffer->bufAddr[0] != NULL);