Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi Team,
I download the CAN example can_ex2_loopback_interrupts from C2000Ware_3_02_00_00 to F28002x control card by CCS10.1, and run the code, see the CAN_IF registers are all zero as below, which should be initialization in the code, what is the problem?