Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello,
Just started programming on F28379D a dual core processor for my motor control project. I have worked quite extensively on F28069M before, so I thought the new device should be easy ....
First I wanted to build a simple CPU project. Placed the led blinking program in my new project. Also as was my previous habit copied the following files into the project directory
xAdc.c,xCodeBranchstart.asm, xdefaulltISR.c, xGlobalVariableDefs.c, xGpio.c, xPieCtrl.c, xPieVect.c, xSyssCtrl.c, xusDealy.asm. Also placed the 2837x_FLASH_lnk_cpu1.cmd into the project.
I have defined CPU1 in the project properties, the compiler does pass this as --define=CPU1 for every source compile.
Now when I build I get the following output. Something is not right. Can you guys help ? Thanks in advance.
Cheers, -Bhaktha
Invoking: C2000 Linker
"C:/ti/ccs920/ccs/tools/compiler/ti-cgt-c2000_18.12.3.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --define=CPU1 -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi -z -m"Chara7KWSrm.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccs920/ccs/tools/compiler/ti-cgt-c2000_18.12.3.LTS/lib" -i"C:/ti/ccs920/ccs/tools/compiler/ti-cgt-c2000_18.12.3.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="Chara7KWSrm_linkInfo.xml" --rom_model -o "Chara7KWSrm.out" "./F2837xD_Adc.obj" "./F2837xD_CodeStartBranch.obj" "./F2837xD_DefaultISR.obj" "./F2837xD_GlobalVariableDefs.obj" "./F2837xD_Gpio.obj" "./F2837xD_PieCtrl.obj" "./F2837xD_PieVect.obj" "./F2837xD_SysCtrl.obj" "./F2837xD_usDelay.obj" "./main.obj" "../2837x_FLASH_lnk_cpu1.cmd" -llibc.a
<Linking>
warning #10247-D: creating output section "EmuBModeVar" without a SECTIONS specification
warning #10247-D: creating output section "EmuBootPinsVar" without a SECTIONS specification
warning #10247-D: creating output section "FlashPumpSemaphoreRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "RomPrefetchRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "RomWaitStateRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cla1SoftIntRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "SyncSocRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "NmiIntruptRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DacaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DacbRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DaccRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "CpuTimer0RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "CpuTimer1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "CpuTimer2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DcsmCommonRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "XintRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "SciaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ScibRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ScicRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ScidRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "SpiaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "SpibRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "SpicRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AdcaResultFile" without a SECTIONS specification
warning #10247-D: creating output section "AdcbResultFile" without a SECTIONS specification
warning #10247-D: creating output section "AdccResultFile" without a SECTIONS specification
warning #10247-D: creating output section "AdcdResultFile" without a SECTIONS specification
warning #10247-D: creating output section "DmaClaSrcSelRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "PieCtrlRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss3RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss4RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss5RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss6RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss7RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cmpss8RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ECap1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ECap2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ECap3RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ECap4RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ECap5RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ECap6RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "InputXbarRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "XbarRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Emif1ConfigRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Emif2ConfigRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EQep1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EQep2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EQep3RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "I2caRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "I2cbRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DcsmZ1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DcsmZ2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "IpcRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "McbspaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "McbspbRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Flash0EccRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "WdRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "GpioDataRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "ClkCfgRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Cla1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwmXbarRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "OutputXbarRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AccessProtectionRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "MemoryErrorRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AnalogSubsysRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "UppRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Emif1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Emif2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AdcaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AdcbRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AdccRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "AdcdRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "MemCfgRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Sdfm1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Sdfm2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "CpuSysRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DmaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm1RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm2RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm3RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm4RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm5RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm6RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm7RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm8RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm9RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm10RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm11RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "EPwm12RegsFile" without a SECTIONS specification
warning #10247-D: creating output section "DevCfgRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "CanaRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "CanbRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "GpioCtrlRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "Flash0CtrlRegsFile" without a SECTIONS specification
warning #10247-D: creating output section "PieVectTableFile" without a SECTIONS specification
Finished building target: "Chara7KWSrm.out"
**** Build Finished ****