Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443
Tool/software: Code Composer Studio
获取不了数据,请问这是为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443
Tool/software: Code Composer Studio
获取不了数据,请问这是为什么?
Hello
Can you please post the question in English
or
Use the following to forum to post this question 
Thank you,
Vaibhav
ok。
MMwave Demo Visualizer - Why can't my IWR1443Boost connect to my computer?
There is the Hardware connected, but the promptis the SDK input version...
I adjusted the baud rate of port 5 to be 115200, but it was 921600 in the lower left corner after I pressed the button, because the maximum baud rate of my computer's port is 128000, I don't know how to solve it。
Hi,
Would you pls help to check with version of IWR1443 is on your board? Is it ES3.0? You can check the mark info in IWR1443 errata to find the silicon version.
Which version of mmWave SDK are you using? And how about the visualizer version?
Hi User,
Can you also confirm you are following the steps in the 14xx Out of Box Demo Lab User Guide?
Thank you for your reply.
At first, I couldn't find the SDK version of 02-01-00-04. I downloaded 02-00-04 and the latest version, and then I downloaded the right one.
Then there is no hint that the SDK version does not match, but there is no relevant data, wating data is always there.
I took a closer look at the baud rate of that port. One port is 115200 and the other is 921600. But I found that the maximum baud rate of my laptop is 128000.
I don't know if that's the reason why I didn't get the data.
Hi User,
Can you confirm you have flashed your board with the correct binaries and have set the device into functional mode after flashing?
Regards,
AG