Part Number: IWR1642BOOST
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: IWR1642BOOST
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
Hello,
From your build snapshot, I notice that you have the MMWAVE SDK installed in C:\ti while CCS is installed in D:\ti. Please install CCS in C:\ti as well and retry the build. If it fails, please provide the build log and snapshot of the failure again.
Regards
-Nitin
It took four hours to generate xwr16xx_ pplcount_ lab.bin.
**** Clean-only build of configuration Debug for project pplcount_16xx_mss ****
"C:\\ti\\ccs930\\ccs\\utils\\bin\\gmake" -k -j 4 clean -O
DEL /F "xwr16xx_pplcount_mss.hex" "configPkg\linker.cmd" "configPkg\compiler.opt" "xwr16xx_pplcount_mss.xer4f"
DEL /F "cli.oer4f" "cycle_measure.oer4f" "gtrackAlloc.oer4f" "gtrackLog.oer4f" "mss_main.oer4f" "radarOsal_malloc.oer4f" "task_app.oer4f" "task_mbox.oer4f"
DEL /F "cli.d" "cycle_measure.d" "gtrackAlloc.d" "gtrackLog.d" "mss_main.d" "radarOsal_malloc.d" "task_app.d" "task_mbox.d"
RMDIR /S/Q "configPkg\"
找不到 D:\Program Files\ccs\workspace_v9\pplcount_16xx_mss\Debug\xwr16xx_pplcount_mss.hex
Finished clean
**** Build Finished ****
**** Build of configuration Debug for project pplcount_16xx_mss ****
"C:\\ti\\ccs930\\ccs\\utils\\bin\\gmake" -k -j 4 all -O
rm -f D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss/xwr16xx_pplcount_mss.bin
makefile:193: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, rm -f D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss/xwr16xx_pplcount_mss.bin, ...) failed.
make (e=2): 系统找不到指定的文件。
gmake[1]: [pre-build] Error 2 (ignored)
Building file: "../mss_mmw.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_50_04_43_core/xs" --xdcpath="C:/ti/bios_6_53_02_00/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.R4F -p ti.platforms.cortexR:IWR16XX:false:200 -r release -c "C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS" --compileOptions "--enum_type=int " "../mss_mmw.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring mss_mmw.xer4f from package/cfg/mss_mmw_per4f.cfg ...
generating custom ti.sysbios library makefile ...
Starting build of library sources ...
making D:/PROGRA~2/ccs/workspace_v9/pplcount_16xx_mss/src/sysbios/sysbios.aer4f ...
gmake[1]: Entering directory `D:/PROGRA~2/ccs/workspace_v9/pplcount_16xx_mss/src/sysbios'
cler4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/BIOS.c ...
asmer4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/family/arm/IntrinsicsSupport_asm.asm ...
asmer4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/family/arm/TaskSupport_asm.asm ...
asmer4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/family/arm/v7r/vim/Hwi_asm.sv7R ...
asmer4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/family/arm/v7r/vim/Hwi_asm_switch.sv7R ...
asmer4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/family/arm/exc/Exception_asm.asm ...
asmer4f C:/ti/bios_6_53_02_00/packages/ti/sysbios/family/arm/v7r/tms570/Core_asm.sv7R ...
arer4f BIOS.obj arm_IntrinsicsSupport_asm.obj arm_TaskSupport_asm.obj vim_Hwi_asm.obj vim_Hwi_asm_switch.obj exc_Exception_asm.obj tms570_Core_asm.obj ...
gmake[1]: Leaving directory `D:/PROGRA~2/ccs/workspace_v9/pplcount_16xx_mss/src/sysbios'
Build of libraries done.
cler4f package/cfg/mss_mmw_per4f.c ...
"package/cfg/mss_mmw_per4f.c", line 17360: warning: statement is unreachable
"package/cfg/mss_mmw_per4f.c", line 17982: warning: statement is unreachable
"package/cfg/mss_mmw_per4f.c", line 18345: warning: statement is unreachable
"package/cfg/mss_mmw_per4f.c", line 18627: warning: statement is unreachable
"package/cfg/mss_mmw_per4f.c", line 18870: warning: statement is unreachable
Finished building: "../mss_mmw.cfg"
Building file: "../cycle_measure.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="cycle_measure.d_raw" --cmd_file="configPkg/compiler.opt" "../cycle_measure.c"
Finished building: "../cycle_measure.c"
Building file: "../gtrackAlloc.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="gtrackAlloc.d_raw" --cmd_file="configPkg/compiler.opt" "../gtrackAlloc.c"
Finished building: "../gtrackAlloc.c"
Building file: "../gtrackLog.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="gtrackLog.d_raw" --cmd_file="configPkg/compiler.opt" "../gtrackLog.c"
Finished building: "../gtrackLog.c"
Building file: "../radarOsal_malloc.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="radarOsal_malloc.d_raw" --cmd_file="configPkg/compiler.opt" "../radarOsal_malloc.c"
Finished building: "../radarOsal_malloc.c"
Building file: "../cli.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="cli.d_raw" --cmd_file="configPkg/compiler.opt" "../cli.c"
Finished building: "../cli.c"
Building file: "../mss_main.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mss_main.d_raw" --cmd_file="configPkg/compiler.opt" "../mss_main.c"
"C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/radarProcess.h", line 58: warning #48-D: incompatible redefinition of macro "M_PI" (declared at line 153 of "C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include/math.h")
Finished building: "../mss_main.c"
Building file: "../task_app.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="task_app.d_raw" --cmd_file="configPkg/compiler.opt" "../task_app.c"
"C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/radarProcess.h", line 58: warning #48-D: incompatible redefinition of macro "M_PI" (declared at line 153 of "C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include/math.h")
Finished building: "../task_app.c"
Building file: "../task_mbox.c"
Invoking: ARM Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="D:/Program Files/ccs/workspace_v9/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_00_00_04" --include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="task_mbox.d_raw" --cmd_file="configPkg/compiler.opt" "../task_mbox.c"
Finished building: "../task_mbox.c"
Building target: "xwr16xx_pplcount_mss.xer4f"
Invoking: ARM Linker
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f -z -m"xwr16xx_pplcount_mss.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/control/mmwave/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/control/mmwavelink/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/crc/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/dma/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/esm/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/gpio/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/mailbox/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/osal/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/pinmux/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/soc/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/drivers/uart/lib" -i"C:/ti/mmwave_sdk_02_00_00_04/packages/ti/utils/cli/lib" -i"C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack/lib" -i"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include" --reread_libs --disable_auto_rts --diag_warning=225 --diag_wrap=off --display_error_number --warn_sections --xml_link_info="xwr16xx_pplcount_mss_linkInfo.xml" --rom_model --unused_section_elimination=on -o "xwr16xx_pplcount_mss.xer4f" "./cli.oer4f" "./cycle_measure.oer4f" "./gtrackAlloc.oer4f" "./gtrackLog.oer4f" "./mss_main.oer4f" "./radarOsal_malloc.oer4f" "./task_app.oer4f" "./task_mbox.oer4f" "../mss_mmw_linker.cmd" "../r4f_linker.cmd" -l"configPkg/linker.cmd" -llibosal_xwr16xx.aer4f -llibesm_xwr16xx.aer4f -llibgpio_xwr16xx.aer4f -llibsoc_xwr16xx.aer4f -llibpinmux_xwr16xx.aer4f -llibcrc_xwr16xx.aer4f -llibdma_xwr16xx.aer4f -llibuart_xwr16xx.aer4f -llibmailbox_xwr16xx.aer4f -llibmmwavelink_xwr16xx.aer4f -llibmmwave_xwr16xx.aer4f -llibcli_xwr16xx.aer4f -llibgtrack_xwr16xx.aer4f -lrtsv7R4_T_le_v3D16_eabi.lib -llibc.a
<Linking>
"C:/ti/mmwave_industrial_toolbox_4_1_0/labs/people_counting/16xx_people_counting/pjt/radarDemo/chains/RadarReceiverPeopleCounting/radarProcess.h", line 58: warning #48-D: incompatible redefinition of macro "M_PI" (declared at line 153 of "C:/ti/ccs930/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS/include/math.h")
Finished building target: "xwr16xx_pplcount_mss.xer4f"
C:/ti/mmwave_sdk_02_00_00_04/packages/scripts/ImageCreator/xwr16xx/out2rprc/out2rprc.exe xwr16xx_pplcount_mss.xer4f xwr16xx_pplcount_mss.bin
Parsing the input object file, xwr16xx_pplcount_mss.xer4f.
Appending zeros 0
Appending zeros 256
Appending zeros 104680
File conversion complete!
C:/ti/mmwave_sdk_02_00_00_04/packages/scripts/ImageCreator/xwr16xx/multicore_image_generator/MulticoreImageGen.exe LE 37 0x00000006 xwr16xx_pplcount_lab.bin 0x35510000 xwr16xx_pplcount_mss.bin 0xb5510000 C:/ti/mmwave_sdk_02_00_00_04/firmware/radarss/xwr16xx_radarss_rprc.bin 0xd5510000 D:/Program Files/ccs/workspace_v9/pplcount_16xx_dss/Debug/xwr16xx_pplcount_dss.bin
Number of Input Files 4
Error opening input image file! D:/Program
Number of zeros 56
Number of zeros 32
Number of zeros 1
C:/ti/mmwave_sdk_02_00_00_04/packages/scripts/ImageCreator/xwr16xx/crc_multicore_image/crc_multicore_image.exe xwr16xx_pplcount_lab.bin xwr16xx_pplcount_lab.bin.tmp
size of App Image is 0 bytes
Padded RPRC Image for Core ID:-716111872
cur_crc_read_addr 128
cur_crc_read_addr 117312
cur_crc_read_addr 139264
Failed to remove CRC temp file
C:/ti/mmwave_sdk_02_00_00_04/packages/scripts/ImageCreator/append_bin_crc/gen_bincrc32.exe xwr16xx_pplcount_lab.bin
>>>> Binary CRC32 = 7e2c186f <<<<
>>>> Total bytes in binary file 139272 <<<<
**** Build Finished ****
However, it encountered an error as shown in the figure below:
I try to use the C:\ti\mmwave_industrial_toolbox_4_1_0\labs\people_counting\16xx_people_counting\quickstart\xwr16xx_pcount_lab.bin.
it can work!
Hello,
It appears that there could be a potential incompatibility/issue caused by CCS 9.3 (could be the ARM compiler 18.x) and we have not built this demo with this version of CCS and hence the newer ARM compiler.
I would suggest you to use the exact CCS version and tools listed in the demo user guide and make sure that it is built with the specified compiler i.e. 16.9.6 in CCS 8.3.1 which is what we used to generate the pre-compiled binary in the demo.
Regards
-Nitin
Re install ccs7.4.0.00015_ After that, the compiler succeeded。
Thank you very much.