Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello there
I am trying to use 2 CPUs same time. I have debugged and run the project 1 in CPU 1 now when I try to debug and run project 2 in CPU 2 then it tells me "stop the existing debug project 1" I have read this link http://dev.ti.com/tirex/explore/node?node=AF77MYXC5GXV9l1NS.Clig__FUz-xrs__LATEST it tells don't debug but load the 2nd project but didn't get the process. Can you please explain the entire process step by step so I can run two projects at the same time on CPU 1 and 2.
Thanks
Avi