Part Number: CODECOMPOSER
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Good morning,
since a few days I have some trouble with getting connection of my USB200 emulator (xds2xx) to my PC. I use Win10 x64 and Code Composer Studio v7.4.0.00015.
If I connect my two USB200 to my PC there are always following error messages:
USB device was not recognized. The last USB device connected to this computer did not work properly and is not recognized by Windows.
On other computers they will be recognized. They are not defect.
If I go to CCS > Help > Installation Details > Installed Software I don't find a line with "TI Emulators".
If I want to "Install New Software..." I can select the line "TI Emulators v8.4.0.0006". At the next step there's an error message:
Cannot complete the install because one or more required items could not be found. Software being installed: TI Emulators 8.4.0.00006 (com.ti.emulation.pack.win32.feature.group 8.4.0.00006) Missing requirement: TI Emulators 8.4.0.00006 (com.ti.emulation.pack.win32.feature.group 8.4.0.00006) requires 'com.ti.ccstudio.installer.win32.feature.group 8.3.1.00004' but it could not be found
I have downloaded "XDS Emulation Software (EMUPack)" from "software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds_software_package_download.html" one after the other and tried to install it:
- 8.2.0.00004 (32-bit Windows (up to CCSv8.3.x))
- 8.3.0.00003 (32-bit Windows (up to CCSv8.3.x))
- 8.4.0.00006 (32-bit Windows (up to CCSv8.3.x))
- 9.2.0.00002 (32-bit Windows (up to CCSv8.3.x))
Every installation fails with following entry in the log files:
[timestamp] Running XDS2xx Driver Installer Executing C:\ti\ccs740/ccs_base/emulation/windows/DPInst64.exe /SE /SW /SA /PATH "C:\ti\ccs740/ccs_base/emulation/windows/xds2xx_drivers" Script exit code: 256 Script output: Script stderr: Program ended with an error exit code Error running C:\ti\ccs740/ccs_base/emulation/windows/DPInst64.exe /SE /SW /SA /PATH "C:\ti\ccs740/ccs_base/emulation/windows/xds2xx_drivers": Program ended with an error exit code
At the moment I have no further ideas and need your support.
Best regards,
Robert