This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Project Unexpectedly (Happily) Starts

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

Greetings,

We have a number of projects which run from various locations in the flash. Using CCS, I have noticed that I can load any of these projects, and it will run to main and stop in the same manner as a project which starts at the reset vector, 0x80000 in this case. This is an unexpected, but welcome behavior. Is this happening because CCS is changing the PC to that project’s starting point?  Is it a feature I can rely upon?

Thank you,

Ed