This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352P: What is the minimum system requirement for EnergyTrace HDR?

Part Number: CC1352P
Other Parts Discussed in Thread: ENERGYTRACE

Tool/software: Code Composer Studio

Hi,

I am having some trouble when trying to run EnergyTrace++ on my not too old laptop (I7-8565U + 16GB RAM + PCIe SSD). Current trace display usually lags quite a bit, while trying to display CPU/peripheral states it usually usually crashes, with error message like the following:

Cortex_M4_0: JTAG Communication Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.2.0.00002)

Or the whole CCS crashes, screenshot attached.

My question is, what is minimum requirement to run EnergyTrace++ hardware wise? I assume the bottleneck is at CPU. Will Ryzen 7 4800U/H be powerful enough? Or something even more powerful is needed?

Thanks.