This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: Error -241

Expert 1995 points

Part Number: TMS570LS3137
Other Parts Discussed in Thread: TMDS570LS31HDK

Tool/software: Code Composer Studio

Hello,

I have the development board TMDS570LS31HDK. 

CCS returns the following error message any time I debug:

Error connecting to the target:
(Error -241 @ 0x0)
A router subpath could not be accessed.
A security error has probably occurred.
Make sure your device is unlocked.
(Emulation package 8.4.0.00006)

The cable works, the drivers are installed and trying the same procedure with an other identical board works.

I tried to scan it with the Dbgjtag utility (Integrity check with reset and reset only); but the 241 error message appears anyway.

I tried to follow the procedure suggested in this post since the error was the same but with another HW; but after creating a configuration file, selecting the target and trying to connect as suggested unfortunately that error appears again and blocks me to continue with the indicated operations.

As last, I tried also with MPROG and the image of the device's eeprom as indicated here for the XDS100v2.

None of the above described operations was successful. Frankly speaking, I am quite surprised that a so expensive equipment (e.g. with respect to the Launchpads) can fail so easily.

Thanks ahead for a solution.

Regards.