Part Number: CC1310
Tool/software: Code Composer Studio
Hello,
I am developing an application for my device based on CC1310. As a starting point, I have used an example project (EasyLink if I am not wrong) from the SDK (4.10) but that example include 2 different projects, one for the actual application and one for the RTOS support library. So I would like to ask if it's possible to merge these two projects into a signle one? If it's not possible, is there any alternative project which already include everything I need to use the RTOS and any other element from the SDK. Note that I don't need to have the EasyLink stack because I have already heavily modified it.
Thank you for your response.