This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

need help on ezdsp f2812, Error 0x00000024/-1166

I,m running BLDC motor by generating pwms from f2812, sensors are hall sensors,

my cpu time period at 100 usec,

i'm getting the folowing error,

Trouble running Target CPU:

Error 0x00000024/-1166 Error during:

Register, Execution,

Lost processor clock. Device may be operating in a low-power mode.

Do you want to bring it out of this mode?

Sequence ID: 16

Error Code: -1166

Error Class: 0x00000024

 

What is this error and how to avoid this?

plz help me..

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

  • ramesh akula said:

    Trouble running Target CPU:

    Error 0x00000024/-1166 Error during:

    Register, Execution,

    Lost processor clock. Device may be operating in a low-power mode.

    Do you want to bring it out of this mode?

    Sequence ID: 16

    Error Code: -1166

    Error Class: 0x00000024

    Is the device indeed going to low power mode after running for a certain amount of time? That is default behavior for some devices if the target runs.

    ki

  • dear ki,

    It is not even running for certain amount of time.

    When ever i connect the motor this error is coming and the dsp is popping a message to disconnect it.

    and now

    Sequence ID: 16

    Error Code: -2074

    Error Class: 0x00000020

    this error is popping up .

    please help me in this regard, my project is struck here.

    regards,

    ramesh.

     

     

     

  •  

    I also had some problems with the "Lost processor clock" on my own motorcontroller application.

    I´m working with an external XDS100 emulator from Spectrum and I get rid of the "lost clock" message after lowering the JTAG - Clock from the default 1 MHz down to (some) 100 kHz.

    Maybe my wiring on my testboard is not perfect shielded and that´s original reason...

    Hope that helps for me and you ;-)

     

    regards,

    Markus

  • hi Markus Schlegel

    i am a master student and i work with F2812 ezdsp

    i have aquestion from you

    please describe for me how i change jtag clock

    thanks