Other Parts Discussed in Thread: 66AK2G12, SYSBIOS
Hi Ki
Thanks for the answers so far. As my interest is to get some reasonably accurate function/thread/CPU load profiling within a rather large DSP application, I think my ETB-only BlackHawk emulator is not going to do the job.
I've moved on to looking into using ROV which I understand makes use of facilities within SYS/BIOS to provide overall CPU loading and thread profiling data. This info would serve me well.
However, I have not yet been able to get ROV to work with my code. When I tried this, while I was successfully connected to my target and the images loaded and running, I was unable to successful connect with ROV. I perused the forum for ROV not connect and found the following thread
The picture in this thread that shows the message Target Not Responding and May Need to be Reset is what I am getting. The end of this thread mentions a bug that Internal teams confirmed and can reproduce. It is not clear if this is my issue or not. Do you have any suggestions? Could I be failing to do some other important step?
I am developing on a 66AK2G12 SoC. Compiler version is v8.2.7. CCS Version: 8.3.1.00004.
Below is a screen shot of my attempt to connect to ROV.