This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352R: ROV: Failed to create the part's controls

Part Number: CC1352R

Tool/software: Code Composer Studio


Hi, 

I'm using CCS v8.3 on Windows 10. When I start the ROV in debug perspective I get the following message: 

Failed to create the part's controls

clicking on "Details" there is: 

com.teamdev.jxbrowser.chromium.internal.ipc.IPCException: IPC process exited. Exit code: -1073741515
	at com.teamdev.jxbrowser.chromium.internal.ipc.d.run(SourceFile:198)
	at java.lang.Thread.run(Thread.java:745)

The same issue appears when I want to launch Resource Explorer and Getting Started. 

Looking in the forum I found that maybe this issue it's related to ./ccs/eclipse/configuration/.jxbrowser-chromium-lib but there is no file such this in this specific directory. 

How can I fix this issue? 


Regards, 
Vincenzo